Hi:) I would like to ask about the use of PWM_Ldd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi:) I would like to ask about the use of PWM_Ldd

917 次查看
priscillayeung
Contributor I

Hi :smileyhappy:

If I want to control the speed of changing LED colours using different position of the touch slider, can I add another pwm ldd to the same led?

Thanks :smileyhappy:

标签 (1)
0 项奖励
回复
1 回复

700 次查看
adriancano
NXP Employee
NXP Employee

Hi,

I do not find necessary adding another pwm component to the LED, you can vary the frequency of the PWM and the duty cycle with the same PWM_LDD component.

You may find useful these post by colleague Erich Styger:

Tutorial: Touching the Freedom KL25Z Board | MCU on Eclipse

Tutorial: PWM with Processor Expert | MCU on Eclipse


Hope this information can help you.

Best Regards,
Adrian

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复