Hi:) I would like to ask about the use of PWM_Ldd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi:) I would like to ask about the use of PWM_Ldd

912 Views
priscillayeung
Contributor I

Hi :smileyhappy:

If I want to control the speed of changing LED colours using different position of the touch slider, can I add another pwm ldd to the same led?

Thanks :smileyhappy:

Labels (1)
0 Kudos
Reply
1 Reply

695 Views
adriancano
NXP Employee
NXP Employee

Hi,

I do not find necessary adding another pwm component to the LED, you can vary the frequency of the PWM and the duty cycle with the same PWM_LDD component.

You may find useful these post by colleague Erich Styger:

Tutorial: Touching the Freedom KL25Z Board | MCU on Eclipse

Tutorial: PWM with Processor Expert | MCU on Eclipse


Hope this information can help you.

Best Regards,
Adrian

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply