Gate Drive Unit Bean

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,831件の閲覧回数
alexit
Contributor I

Is there a GDU bean in one of the advanced (paid) toolsets?

Thanks,

D

0 件の賞賛
返信
1 解決策
3,657件の閲覧回数
bogdannitu-b454
NXP Employee
NXP Employee

Please download and install over CW MCU 10.5 "CW MCU v10.4 S12ZVM Service Pack" from

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_10_4

Best regards,

Bogdan

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,657件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

could you please provide more details? What family, MCU are you targeting?

Best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信
3,657件の閲覧回数
alexit
Contributor I

I am looking at the MC9S12ZVM.

Thanks,

D

0 件の賞賛
返信
3,657件の閲覧回数
bogdannitu-b454
NXP Employee
NXP Employee

Hello,

You may use Init_GDU component for MC9S12ZVM.

Best regards,

Bogdan

0 件の賞賛
返信
3,657件の閲覧回数
alexit
Contributor I

I have CW 10.5 with the PEx Core Update (1.0.1) and the S12Z service pack (1.0.2) installed. The Init_GDU component does not appear in my lists, do I need an advanced library to receive this? If yes, which one do I purchase?

Thanks,

D.

0 件の賞賛
返信
3,658件の閲覧回数
bogdannitu-b454
NXP Employee
NXP Employee

Please download and install over CW MCU 10.5 "CW MCU v10.4 S12ZVM Service Pack" from

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_10_4

Best regards,

Bogdan

0 件の賞賛
返信