Failure when generatin Processor Expert code for MagniV S12ZVCA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failure when generatin Processor Expert code for MagniV S12ZVCA

Jump to solution
6,148 Views
maxdrm
Contributor II

Hello!

When I run "Generate Processor Expert Code" I get the following error:

     Generator: FAILURE: Unexpected status of script: Drivers\HCS12\ADC_withLBA.drv, please contact Freescale      support. Pcm_V1.0.0a0        AD1 Processor Expert Problem.

Any help would be helpful.

Labels (1)
0 Kudos
Reply
1 Solution
5,662 Views
maxdrm
Contributor II

Hello Bogdan, now it works with CW 10.6.4.

Thank You

Max

View solution in original post

0 Kudos
Reply
4 Replies
5,662 Views
bogdannitu-b454
NXP Employee
NXP Employee

Hello,

Could you please send your project where you reproduce this issue?

Please specify the version of Code Warrior.

Best regards,

Bogdan

0 Kudos
Reply
5,653 Views
maxdrm
Contributor II

Hello Bogdan,

the CodeWarrior version is 10.6, see below for details.

In the allegate file there is the project where the fault occurs.

Have a nice day

Max

Da: bogdannitu-b45429

Inviato: giovedì 26 maggio 2016 18:03

A: Di Ruggiero Massimiliano

Oggetto: Re: - Failure when generatin Processor Expert code for MagniV S12ZVCA

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Failure when generatin Processor Expert code for MagniV S12ZVCA

reply from Bogdan Nitu<https://community.nxp.com/people/bogdannitu-b45429?et=watches.email.thread> in Processor Expert Software - View the full discussion<https://community.nxp.com/message/654792?et=watches.email.thread#comment-654792>

0 Kudos
Reply
5,653 Views
bogdannitu-b454
NXP Employee
NXP Employee

Hello Max,

PEx for S12ZVCA is supported in Code Warrior starting with CW 10.6.4.

Best regards,

Bogdan

0 Kudos
Reply
5,663 Views
maxdrm
Contributor II

Hello Bogdan, now it works with CW 10.6.4.

Thank You

Max

0 Kudos
Reply