Failure when generatin Processor Expert code for MagniV S12ZVCA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failure when generatin Processor Expert code for MagniV S12ZVCA

ソリューションへジャンプ
6,215件の閲覧回数
maxdrm
Contributor II

Hello!

When I run "Generate Processor Expert Code" I get the following error:

     Generator: FAILURE: Unexpected status of script: Drivers\HCS12\ADC_withLBA.drv, please contact Freescale      support. Pcm_V1.0.0a0        AD1 Processor Expert Problem.

Any help would be helpful.

ラベル(1)
0 件の賞賛
返信
1 解決策
5,729件の閲覧回数
maxdrm
Contributor II

Hello Bogdan, now it works with CW 10.6.4.

Thank You

Max

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,729件の閲覧回数
bogdannitu-b454
NXP Employee
NXP Employee

Hello,

Could you please send your project where you reproduce this issue?

Please specify the version of Code Warrior.

Best regards,

Bogdan

0 件の賞賛
返信
5,720件の閲覧回数
maxdrm
Contributor II

Hello Bogdan,

the CodeWarrior version is 10.6, see below for details.

In the allegate file there is the project where the fault occurs.

Have a nice day

Max

Da: bogdannitu-b45429

Inviato: giovedì 26 maggio 2016 18:03

A: Di Ruggiero Massimiliano

Oggetto: Re: - Failure when generatin Processor Expert code for MagniV S12ZVCA

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Failure when generatin Processor Expert code for MagniV S12ZVCA

reply from Bogdan Nitu<https://community.nxp.com/people/bogdannitu-b45429?et=watches.email.thread> in Processor Expert Software - View the full discussion<https://community.nxp.com/message/654792?et=watches.email.thread#comment-654792>

0 件の賞賛
返信
5,720件の閲覧回数
bogdannitu-b454
NXP Employee
NXP Employee

Hello Max,

PEx for S12ZVCA is supported in Code Warrior starting with CW 10.6.4.

Best regards,

Bogdan

0 件の賞賛
返信
5,730件の閲覧回数
maxdrm
Contributor II

Hello Bogdan, now it works with CW 10.6.4.

Thank You

Max

0 件の賞賛
返信