FSL_USB_CDC_Device support for K20?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FSL_USB_CDC_Device support for K20?

Jump to solution
3,326 Views
bowerymarc
Contributor V

I noticed the FSL_USB_CDC_Device doesn't include the K20 in it's drop down for processor type.... will that be supported anytime? Or can I just pick K40 or K60?

Labels (1)
0 Kudos
Reply
1 Solution
2,982 Views
BlackNight
NXP Employee
NXP Employee

Hi Marc,

K20 (FRDM-K20D50M, 50 MHz) is now supported:

USB CDC with the FRDM-K20D50M | MCU on Eclipse

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
5 Replies
2,983 Views
BlackNight
NXP Employee
NXP Employee

Hi Marc,

K20 (FRDM-K20D50M, 50 MHz) is now supported:

USB CDC with the FRDM-K20D50M | MCU on Eclipse

I hope this helps,

Erich

0 Kudos
Reply
2,982 Views
bowerymarc
Contributor V

cool... so for experimenting the TWR-K20D50M could be used...  for the product I'm using the K20F120...

0 Kudos
Reply
2,982 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

you need install USB CDC Class componet first from USB stack 4.03. disable "Filter" button you will see all the component aviable for pocessor expert.

see screeshotUSB CDC class.JPG

the "Filter " only show component avaiable for processor in foucus project.

Best Regards,

Jennie

2,982 Views
kooroshhajiani
Contributor III

Hi,

I'm trying to use processor expert to build a USB CDC DEVICE  for k20 target board. I can not see USB CDC class under the component for this target. I'm using KDS 3.1.0 + DSK1.3.1

Any ideas?

Thanks,

Koorosh Hajiani

0 Kudos
Reply
2,982 Views
BlackNight
NXP Employee
NXP Employee

I have not had a chance to add it, but it is definitely on my list. I plan to do it with the FRDM-K20D50M.

You might give it a try with the K40, but I have not verified if this works with the K20.

0 Kudos
Reply