FSL_USB_CDC_Device support for K20?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FSL_USB_CDC_Device support for K20?

ソリューションへジャンプ
3,616件の閲覧回数
bowerymarc
Contributor V

I noticed the FSL_USB_CDC_Device doesn't include the K20 in it's drop down for processor type.... will that be supported anytime? Or can I just pick K40 or K60?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,272件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Marc,

K20 (FRDM-K20D50M, 50 MHz) is now supported:

USB CDC with the FRDM-K20D50M | MCU on Eclipse

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,273件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Marc,

K20 (FRDM-K20D50M, 50 MHz) is now supported:

USB CDC with the FRDM-K20D50M | MCU on Eclipse

I hope this helps,

Erich

0 件の賞賛
返信
3,272件の閲覧回数
bowerymarc
Contributor V

cool... so for experimenting the TWR-K20D50M could be used...  for the product I'm using the K20F120...

0 件の賞賛
返信
3,272件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

you need install USB CDC Class componet first from USB stack 4.03. disable "Filter" button you will see all the component aviable for pocessor expert.

see screeshotUSB CDC class.JPG

the "Filter " only show component avaiable for processor in foucus project.

Best Regards,

Jennie

3,272件の閲覧回数
kooroshhajiani
Contributor III

Hi,

I'm trying to use processor expert to build a USB CDC DEVICE  for k20 target board. I can not see USB CDC class under the component for this target. I'm using KDS 3.1.0 + DSK1.3.1

Any ideas?

Thanks,

Koorosh Hajiani

0 件の賞賛
返信
3,272件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I have not had a chance to add it, but it is definitely on my list. I plan to do it with the FRDM-K20D50M.

You might give it a try with the K40, but I have not verified if this works with the K20.

0 件の賞賛
返信