FSL_USB_CDC_Device support for K20?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FSL_USB_CDC_Device support for K20?

跳至解决方案
3,447 次查看
bowerymarc
Contributor V

I noticed the FSL_USB_CDC_Device doesn't include the K20 in it's drop down for processor type.... will that be supported anytime? Or can I just pick K40 or K60?

标签 (1)
0 项奖励
回复
1 解答
3,103 次查看
BlackNight
NXP Employee
NXP Employee

Hi Marc,

K20 (FRDM-K20D50M, 50 MHz) is now supported:

USB CDC with the FRDM-K20D50M | MCU on Eclipse

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,104 次查看
BlackNight
NXP Employee
NXP Employee

Hi Marc,

K20 (FRDM-K20D50M, 50 MHz) is now supported:

USB CDC with the FRDM-K20D50M | MCU on Eclipse

I hope this helps,

Erich

0 项奖励
回复
3,103 次查看
bowerymarc
Contributor V

cool... so for experimenting the TWR-K20D50M could be used...  for the product I'm using the K20F120...

0 项奖励
回复
3,103 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

you need install USB CDC Class componet first from USB stack 4.03. disable "Filter" button you will see all the component aviable for pocessor expert.

see screeshotUSB CDC class.JPG

the "Filter " only show component avaiable for processor in foucus project.

Best Regards,

Jennie

3,103 次查看
kooroshhajiani
Contributor III

Hi,

I'm trying to use processor expert to build a USB CDC DEVICE  for k20 target board. I can not see USB CDC class under the component for this target. I'm using KDS 3.1.0 + DSK1.3.1

Any ideas?

Thanks,

Koorosh Hajiani

0 项奖励
回复
3,103 次查看
BlackNight
NXP Employee
NXP Employee

I have not had a chance to add it, but it is definitely on my list. I plan to do it with the FRDM-K20D50M.

You might give it a try with the K40, but I have not verified if this works with the K20.

0 项奖励
回复