Error: This component not supported in Kinetis SDK Project mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error: This component not supported in Kinetis SDK Project mode

1,568件の閲覧回数
tomtalkington
Contributor III

I am attempting to add a PWM component and am getting this error I also get it when attempting to add a Timer component.  What exactly does it mean?

ラベル(1)
0 件の賞賛
返信
1 返信

1,169件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tom Talkington:

Was the project created with "KSDK" option enabled in the New Project Wizard?

If so, as the error indicates the LDD components cannot be used in KSDK + Processor Expert projects, instead you have the fsl_xxx components.

There are some discussions in the community about this topic:

Re: How do I merge PEx components from PEx DriverSuite into KDS/SDK?

Re: KSDK and the old PEx (non-KSDK) compatibility

Re: MQX vs MQX Lite?


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信