ENGR00297465

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ENGR00297465

1,602件の閲覧回数
geoffreyduddrid
Contributor I

CW10.6 release notes refer to a Processor Expert bug fix as follows:

"ENGR00297465 – Fixed Processor Expert EnterCritical() and ExitCritical() macro implementation for Kinetis family."

I am still using CW10.4 for a Kinetis K20. Is there any way to get more info so I can decided if I need to manually address this bug or consider upgrading to 10.6?

thanks!

ラベル(2)
0 件の賞賛
返信
1 返信

1,265件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Geo,

I recommend you use the latest version CW10.6.6 (cw10.6.4 with update 6) ,

for the the new one have fixed bugs that old one have , and also have some updates.

And you can also use the KDS3.0 , it also have the Processor Expert , this IDE is free,

you can download and install refer to here :

New Kinetis Design Studio V3.0.0 available

The KSDK1.3 is a kinetis development kit .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信