Difference between kernel branches in github.com/Freescale/linux-fslc repository

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between kernel branches in github.com/Freescale/linux-fslc repository

ソリューションへジャンプ
4,032件の閲覧回数
rspolyak
Contributor II

Repo https://github.com/Freescale/linux-fslc has branches that ends with -imx and branches that ends with -fslc. I suppose that -imx are official Freescale kernels whereas -fslc are supported by community. Are -imx branches merged to -fslc?

Currently I am using Yocto Dunfell with 5.4.x+fslc branch. However this branch does not include folder drivers/video/fbdev/mxc that contains video drivers that I need. On the other hand 5.4-2.1.x-imx does include this folder.

0 件の賞賛
返信
1 解決策
4,003件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

nxp does not support linux-fslc, please post this on meta-fsl-arm mailing list

https://lists.yoctoproject.org/g/meta-freescale

 

Best regards
igor

元の投稿で解決策を見る

4 返答(返信)
4,024件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信
4,006件の閲覧回数
rspolyak
Contributor II

According to https://www.yoctoproject.org/pipermail/meta-freescale/2018-August/023214.html there is a branch `linux-fslc-imx` which include both community and iMX changes. However I do not see this branch neither at https://github.com/Freescale/linux-fslc/ nor at https://source.codeaurora.org/external/imx/linux-imx.

Is this information still up to date?

0 件の賞賛
返信
4,004件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

nxp does not support linux-fslc, please post this on meta-fsl-arm mailing list

https://lists.yoctoproject.org/g/meta-freescale

 

Best regards
igor

4,030件の閲覧回数
rspolyak
Contributor II

If I understood correctly, MXS video driver was removed in 5.3 kernel: https://patchwork.kernel.org/project/dri-devel/patch/[email protected]/

Any examples how to port MXS based video driver to DRM version?

0 件の賞賛
返信