Configuring OPWM using EMIOS on MPC5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring OPWM using EMIOS on MPC5777C

ソリューションへジャンプ
3,023件の閲覧回数
ikarkala
Contributor III

Hi,

 

I am trying to configure an EMIOS channel in OPWM mode . I wanted to know if there is a way to configure it for a fixed amount of time . Example : configuring it in at 5Mhz frequency for 4 seconds ?

Regards,

Indy

0 件の賞賛
返信
1 解決策
2,990件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no such mode is supported by HW in single channel. Output disable  (ODIS) feature can be used, when flag of another channel can disable channel output. Thus another channel can count that 4sec delay and after that disable PWM output of channel with ODIS enabled (but PWM still run).
Or you need to use SW way to stop PWM channel.

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,991件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no such mode is supported by HW in single channel. Output disable  (ODIS) feature can be used, when flag of another channel can disable channel output. Thus another channel can count that 4sec delay and after that disable PWM output of channel with ODIS enabled (but PWM still run).
Or you need to use SW way to stop PWM channel.

BR, Petr

0 件の賞賛
返信
2,985件の閲覧回数
ikarkala
Contributor III
Thank you
0 件の賞賛
返信