Configuring OPWM using EMIOS on MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring OPWM using EMIOS on MPC5777C

Jump to solution
3,037 Views
ikarkala
Contributor III

Hi,

 

I am trying to configure an EMIOS channel in OPWM mode . I wanted to know if there is a way to configure it for a fixed amount of time . Example : configuring it in at 5Mhz frequency for 4 seconds ?

Regards,

Indy

0 Kudos
Reply
1 Solution
3,004 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no such mode is supported by HW in single channel. Output disable  (ODIS) feature can be used, when flag of another channel can disable channel output. Thus another channel can count that 4sec delay and after that disable PWM output of channel with ODIS enabled (but PWM still run).
Or you need to use SW way to stop PWM channel.

BR, Petr

View solution in original post

0 Kudos
Reply
2 Replies
3,005 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no such mode is supported by HW in single channel. Output disable  (ODIS) feature can be used, when flag of another channel can disable channel output. Thus another channel can count that 4sec delay and after that disable PWM output of channel with ODIS enabled (but PWM still run).
Or you need to use SW way to stop PWM channel.

BR, Petr

0 Kudos
Reply
2,999 Views
ikarkala
Contributor III
Thank you
0 Kudos
Reply