CAN_LDD, how to use ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN_LDD, how to use ?

5,216件の閲覧回数
kentachang
Contributor I

Hello,

I hope to use CAN_LDD for CAN bus transceiver, but I do not know How to setting the CAN_LDD component?

attachment is my project, please let me know ...

 

Best Regards,

Kenta 

Original Attachment has been moved to: _K60_DN512__CAN_LDD.rar

0 件の賞賛
返信
3 返答(返信)

4,563件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Kenta,

I think you can refer CAN_LDD sample code under {CW10.6 install}\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K60N512\CAN

====================================

this answer is for you. if it helps,please click on "correct answer" button. thanks!

Best Regards.

ZhangJun

4,562件の閲覧回数
kentachang
Contributor I

Hi Jennie,

I see the TWR-K60N512/CAN example project and  modify my project(attached). I want to let CAN0 module to repeat transmit messages and receive messages.

Can you help me to modify or correct my project? Let it to send messages and read messages.

Best regards,

Kenta

0 件の賞賛
返信

4,560件の閲覧回数
kentachang
Contributor I

Hi Jennie,

I find a circuit on the page 200 AN2865 is good for me.

Is there a MK60 example code like AN2865 ?

and What value is the resistor ?  the power supply will be 3.3V not 5.0V

please ...

Kenta  

0 件の賞賛
返信