Bootloader and EEPROM NVMFlex with K20

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader and EEPROM NVMFlex with K20

1,532件の閲覧回数
night
Contributor II

Hi,

I'm trying to use bootloader with EEProm over NVMFlex memory. The application works fine without the bootloader but when I work with bootloader I can't write on the EEPROM. I just enabled the Partitioning for device register on advanced options in the project menu. The code value used with this is 3303 (for use 2KB eeprom). With the bootloader project I use the same configuration but it doesn't work. Where is the problem?

Thank you and sorry for my English.

Best Regards,

          Miguel Ángel.

ラベル(1)
0 件の賞賛
返信
1 返信

1,365件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

we would need more deatils about the bootloader. Could you please provide more details of the project or in the best case some project how to reproduce it?

best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信