Ask sample code about using Procssor Expert with FreescaleCAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ask sample code about using Procssor Expert with FreescaleCAN

Jump to solution
1,955 Views
rexliao_tw
Contributor I

Dear Sir,

In below discussion thread, you mention about a sample code which does a simple "bridge" between SCI and CAN (MSCAN) with using FreescaleCAN.

Need your help:How can I access MSCAN with Processor Expert

Could you kindly advise where can download this sample project?

Thanks a lot.

BR,

Rex Liao

0 Kudos
Reply
1 Solution
1,849 Views
Petr_H
NXP Employee
NXP Employee

Hi,

I have just added the project into the original thread.

It was probably accidentally removed during the discussion data migration. Sorry for an inconvenience.

best regards

Petr Hradsky

Processor Expert Support Team

View solution in original post

0 Kudos
Reply
2 Replies
1,850 Views
Petr_H
NXP Employee
NXP Employee

Hi,

I have just added the project into the original thread.

It was probably accidentally removed during the discussion data migration. Sorry for an inconvenience.

best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply
1,849 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

if you use CW for HCS12x v5.1,

There is an example project using FreescaleCAN component in the CodeWarrior installation path.

You can find it under Processor Expert\Projects\Test projects\CAN

Example path:

C:\Program Files\Freescale\CWS12 vx.x\ProcessorExpert\Projects\Test projects\CAN

I also attached it.

0 Kudos
Reply