Ask sample code about using Procssor Expert with FreescaleCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ask sample code about using Procssor Expert with FreescaleCAN

ソリューションへジャンプ
1,897件の閲覧回数
rexliao_tw
Contributor I

Dear Sir,

In below discussion thread, you mention about a sample code which does a simple "bridge" between SCI and CAN (MSCAN) with using FreescaleCAN.

Need your help:How can I access MSCAN with Processor Expert

Could you kindly advise where can download this sample project?

Thanks a lot.

BR,

Rex Liao

0 件の賞賛
返信
1 解決策
1,791件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

I have just added the project into the original thread.

It was probably accidentally removed during the discussion data migration. Sorry for an inconvenience.

best regards

Petr Hradsky

Processor Expert Support Team

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,792件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

I have just added the project into the original thread.

It was probably accidentally removed during the discussion data migration. Sorry for an inconvenience.

best regards

Petr Hradsky

Processor Expert Support Team

0 件の賞賛
返信
1,791件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

if you use CW for HCS12x v5.1,

There is an example project using FreescaleCAN component in the CodeWarrior installation path.

You can find it under Processor Expert\Projects\Test projects\CAN

Example path:

C:\Program Files\Freescale\CWS12 vx.x\ProcessorExpert\Projects\Test projects\CAN

I also attached it.

0 件の賞賛
返信