Android 13 Source code - Build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android 13 Source code - Build error

11,122 次查看
Adi99
Contributor I

I have downloaded source code from nxp website for imx8mp - Android 13 code.

but when I start to build bootloader for imx8mp-evk user debug image i got below error .

******************************************************************************************************

Compiling mkimage_imx8
PLAT=imx8mp HDMI=no
make[2]: *** No rule to make target 'lpddr4_pmu_train_1d_imem_202006.bin', needed by 'u-boot-spl-ddr.bin'. Stop.
make[2]: *** Waiting for unfinished jobs....
Compiling mkimage_imx8
cc -O2 -Wall -std=c99 -static ../iMX8M/mkimage_imx8.c -o mkimage_imx8 -lz
../iMX8M/mkimage_imx8.c: In function ‘copy_file.constprop’:
../iMX8M/mkimage_imx8.c:345:21: warning: ‘write’ reading 5 bytes from a region of size 4 [-Wstringop-overread]
345 | if (write(ifd, (char *)&zero, 4-tail) != 4-tail) {
| ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
../iMX8M/mkimage_imx8.c:303:13: note: source object ‘zero’ of size 4
303 | int zero = 0;
| ^~~~
In file included from ../iMX8M/mkimage_imx8.c:24:
/usr/include/unistd.h:378:16: note: in a call to function ‘write’ declared with attribute ‘access (read_only, 2, 3)’
378 | extern ssize_t write (int __fd, const void *__buf, size_t __n) __wur
| ^~~~~
make[1]: *** [Makefile:23: flash_evk] Error 2

 

 

what is the problem?

0 项奖励
回复
12 回复数

9,819 次查看
GixKi
Contributor III

hi,
I am trying to do the same thing.
I am following the directions given in this document:
https://www.nxp.com/docs/en/user-guide/Android_Auto_User's_Guide.pdf

however i see that the “build” folder is not created with the envsetup.sh file

could you give me some pointers?

thanks

0 项奖励
回复

9,773 次查看
GixKi
Contributor III

i solved the problem: it was a misconfiguration of the enterprise network architecture

标记 (1)
0 项奖励
回复

8,430 次查看
zhangzm
Contributor II

How did you solve it?

thanks

0 项奖励
回复

8,419 次查看
GixKi
Contributor III
The problem was in the download phase of the android source code. The corporate IT department had applied restrictions, so the source code had not been downloaded correctly. Once these restrictions were removed from the firewall by the IT department, I was able to do the build correctly. I hope I was of some help.
0 项奖励
回复

8,405 次查看
zhangzm
Contributor II

OK. Thanks!

0 项奖励
回复

11,094 次查看
Adi99
Contributor I

HI @Zhiming_Liu 

1. source build/envsetup.sh

export CLANG_PATH=/opt/prebuilt-android-clang

export AARCH64_GCC_CROSS_COMPILE=/opt/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu-

2. lunch evk_8mp-userdebug

3. ./imx-make.sh bootloader -j24

 

steps i have checked is up to date. but it will throw same error.

 

../iMX8M/mkimage_imx8.c: In function ‘copy_file.constprop’:
../iMX8M/mkimage_imx8.c:345:21: warning: ‘write’ reading 5 bytes from a region of size 4 [-Wstringop-overread]
345 | if (write(ifd, (char *)&zero, 4-tail) != 4-tail) {
| ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
../iMX8M/mkimage_imx8.c:303:13: note: source object ‘zero’ of size 4
303 | int zero = 0;
| ^~~~
In file included from ../iMX8M/mkimage_imx8.c:24:

0 项奖励
回复

11,082 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Do you still have this issue?

make[2]: *** No rule to make target 'lpddr4_pmu_train_1d_imem_202006.bin', needed by 'u-boot-spl-ddr.bin'. Stop.
make[2]: *** Waiting for unfinished jobs....

Maybe your repo sync is not complete and miss this firmware. 

0 项奖励
回复

11,062 次查看
Adi99
Contributor I

Hi @Zhiming_Liu 

error: bootable/libbootloader/: platform/bootable/libbootloader checkout 3dccc2dc55b1982668c268cefc1f648e489519a4
error: Cannot checkout platform/bootable/libbootloader

error: Unable to fully sync the tree.
error: Checking out local projects failed.
Failing repos:
bootable/libbootloader
Try re-running with "-j1 --fail-fast" to exit at the first error.

 

repo sync fialure in bootloader part. I have tried 4 to 5 times repo sync -j1 --fail-fast but same error is throwing.

what is the solution for that?

0 项奖励
回复

11,039 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

@Adi99 

Try to delete the repo workspace and repo init again.

0 项奖励
回复

11,078 次查看
Adi99
Contributor I

Hi @Zhiming_Liu 

 

yes same error getting. again check repo sync and update you.

Thanks.

0 项奖励
回复

11,106 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

@Adi99 

Please share your detailed steps. It seems that the product name you input is not correct.The correct command should be lunch evk8_mp-userdebug

0 项奖励
回复

10,791 次查看
Adi99
Contributor I

Hi @Zhiming_Liu 

 

i have solved this issue. I have re downloaded again repo and follow that NXP guide its works successfully.

0 项奖励
回复