Add missing cpu variant MK20DX256VMC7 (MAPBGA 121 pin)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Add missing cpu variant MK20DX256VMC7 (MAPBGA 121 pin)

2,414件の閲覧回数
lategoodbye
Senior Contributor I

Hi,

i have the following problem in Processor Expert in Code Warrior 10.3. I want to use the MK20DX256VMC7 (MAPBGA, 121 pin), but this variant isn't unavailable in Processor Expert only variants with less pins.

Which variant would be the closest fit?

Is there any way to add support manually for CodeWarrior?

Are there any plans to add 121-MAPBGA packages in the next MCUs Driver Suite for Processor Expert?

Thanks in advance.


ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,014件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

we are sorry for inconvenience, currently the 121-MAPBGA package is not supported. But we plan to support it in future. Maybe by the end of this year...

As "workaround" I would recommend to use 100LQFP package.

best regards

Vojtech Filip

Processor Expert Support Team


0 件の賞賛
返信

2,014件の閲覧回数
lategoodbye
Senior Contributor I

Hi,

a year has gone by and i want to know about are there any plans to integrate MK20DX256VMC7 into processor expert?

Best regards

Stefan Wahren

0 件の賞賛
返信

2,014件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hi Stefan,

We are sorry for the inconvenience. It has been decided by management that this  CPU variant will not be supported by Processor Expert now.

Best Regards,

Marek Neuzil

0 件の賞賛
返信