I try to generate code for a MKL25Z128VLK4 with processor expert. I have added the Serial_LDD. But I can't find where it sets the SIM_SOPT2[UART0SRC]. SIM_SOPT2[PLLFLLSEL] is set.
Is there a bug in PE?
/* SIM_SOPT2: PLLFLLSEL=1 */
SIM_SOPT2 |= SIM_SOPT2_PLLFLLSEL_MASK; /* Select PLL as a clock source for various peripherals */
/* SIM_SOPT1: OSC32KSEL=3 */
SIM_SOPT1 |= SIM_SOPT1_OSC32KSEL(0x03); /* LPO 1kHz oscillator drives 32 kHz clock for various peripherals */
/* SIM_SOPT2: TPMsrc=1 */
SIM_SOPT2 = (uint32_t)((SIM_SOPT2 & (uint32_t)~(uint32_t)(
SIM_SOPT2_TPMSRC(0x02)
)) | (uint32_t)(
SIM_SOPT2_TPMSRC(0x01)
)); /* Set the TPM clock */
Solved! Go to Solution.
Found it :-)
UART0_PDD_SetClockSource(UART0_BASE_PTR, UART0_PDD_PLL_FLL_CLOCK);
So no bug.
Found it :-)
UART0_PDD_SetClockSource(UART0_BASE_PTR, UART0_PDD_PLL_FLL_CLOCK);
So no bug.