MC33816 current filter in asynchronous mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33816 current filter in asynchronous mode

4,321件の閲覧回数
johrehn
Contributor II

Hi!

When running the DC-DC converter on MC33816 in asynchronous mode, is the internal circuitry applying filtering using registers values "filter_length_4l" and "filter_length_4h"?

Reference manual says "The six current feedbacks are filtered before feeding them to the microcore" about the current filter registers. That together with results from our experiments suggests that filters are only applied when reading current sensors from microcode, but it would nice to have that confirmed so that we can eliminate incorrect configuration as an explanation for the behavior we're seeing.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

4,269件の閲覧回数
philippe_meunie
NXP Employee
NXP Employee

Hello Johrehn,

This is true, it is not included in our data sheet, it comes from an internal document.

Cordially,

Philippe

0 件の賞賛
返信

4,298件の閲覧回数
philippe_meunie
NXP Employee
NXP Employee

Hello Tomas,

I can confirm that unfiltered comparator outputs are used for the asynchonous mode of operation, as shown in enclosed picture.

Cordially,
Philippe

4,291件の閲覧回数
johreh
Contributor I

Thank you Philippe.

From which document is the picture taken? I did not see it when reading the reference manual.

0 件の賞賛
返信