MC33816 current filter in asynchronous mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC33816 current filter in asynchronous mode

4,346 次查看
johrehn
Contributor II

Hi!

When running the DC-DC converter on MC33816 in asynchronous mode, is the internal circuitry applying filtering using registers values "filter_length_4l" and "filter_length_4h"?

Reference manual says "The six current feedbacks are filtered before feeding them to the microcore" about the current filter registers. That together with results from our experiments suggests that filters are only applied when reading current sensors from microcode, but it would nice to have that confirmed so that we can eliminate incorrect configuration as an explanation for the behavior we're seeing.

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

4,294 次查看
philippe_meunie
NXP Employee
NXP Employee

Hello Johrehn,

This is true, it is not included in our data sheet, it comes from an internal document.

Cordially,

Philippe

0 项奖励
回复

4,323 次查看
philippe_meunie
NXP Employee
NXP Employee

Hello Tomas,

I can confirm that unfiltered comparator outputs are used for the asynchonous mode of operation, as shown in enclosed picture.

Cordially,
Philippe

4,316 次查看
johreh
Contributor I

Thank you Philippe.

From which document is the picture taken? I did not see it when reading the reference manual.

0 项奖励
回复