Load some data into the Data RAM memory in MC33PT2000?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Load some data into the Data RAM memory in MC33PT2000?

Jump to solution
5,728 Views
Borden
Contributor III

MC33PT2000, During program execution, need to modify some data in DATARAM. While debugging, it was discovered that rewriting all 192 data  to DATARAM was the only effective method. Is it possible to change a specific data in DATARAM Using a simple method? How can the code be written?

DataRAMChangeData.png

Labels (1)
0 Kudos
Reply
1 Solution
5,686 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Hongyu,

please use the PSC simulator. Please check the videos in this link. Please also check the section 8.1.2.2 in the PT2000 datasheet.

JozefKozon_0-1725346627507.png

 

With Best Regards,

Jozef

View solution in original post

4 Replies
5,709 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Hongyu,

the DataRAM access is described in the section 2.8 in the PT2000SWUG attached. Please refer to it.

With Best Regards,

Jozef

0 Kudos
Reply
5,692 Views
Borden
Contributor III
Thank you! But, I didn't describe it clearly. Actually, I want to enable real-time data exchange between the microcontroller (for example: S32K144) and the MC33PT2000 (writing data to DATARAM). What method should I use?
0 Kudos
Reply
5,687 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Hongyu,

please use the PSC simulator. Please check the videos in this link. Please also check the section 8.1.2.2 in the PT2000 datasheet.

JozefKozon_0-1725346627507.png

 

With Best Regards,

Jozef

5,677 Views
Borden
Contributor III
Thanks!
0 Kudos
Reply