HB2000 status value error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HB2000 status value error

5,487件の閲覧回数
hyjung
Contributor II

Dear all.

I have a question to ask about the MC33HB2000 about fault detection.

1. test setup

 -. Used as H-bridge mode & Parallel mode with Vpwr 12V.

 -. Set the initial SPI default value and run after Out 1 & out 2 short.

  2. Read motor driver status value
  -. case 1) 0x2001
  -. case 2) 0x2194

Question)

As a result of repeatedly checking the motor status value under the same conditions,

different fault value appears, and we inquire about the reason. 

Thanks.

0 件の賞賛
返信
5 返答(返信)

5,356件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

How to understand about OUT1&OUT2 short? they are short together?

What's the register setting of Fault status mask register?

Or what about work normally then short OUT1/OUT2 to read fault register normal or not?

0 件の賞賛
返信

5,356件の閲覧回数
hyjung
Contributor II

Thank you response.

OUT1 & OUT2 are connected by wire, not by motor

Fault status mask is default setting.

The same register is while the motor is running, 0x2001 occurs frequently in the reverse direction, 

and 0x2194 occurs frequently inthe forward direction.

Thanks.

0 件の賞賛
返信

5,356件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

I attached the short circuit application note for more explain here.

If short OUT1 and OUT2 the over current will happened,at last over temperature also happen to trigger.

0 件の賞賛
返信

5,356件の閲覧回数
hyjung
Contributor II

Thank you for your response.

When OUT1 and OUT2 are set to short and operate at normal temperature, OT occurs immediately, and the Tj of the device does not exceed OT.
Does it mean that OT shutdown does not correlate with Tj temperature?

Thanks

0 件の賞賛
返信

5,356件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

If so please suggest customer to do same test in NXP evb KIT to eliminate hardware issue.

0 件の賞賛
返信