Does SPIGen have a interface with LABView on MC33816?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does SPIGen have a interface with LABView on MC33816?

1,699 次查看
shuaiyue
Contributor I


Hey guys. I new to KIT 33816 board and I am using it to do the injection and control the pumping control valve. Now, I want to control the behavior of injection and pumping control valve in LABView since some feedback signals which are used to do a closed loop control come into the LABView. But here is problem, how can I run different single command or batch command automatically after I change the parameters in the configuration registers?

 

Best regards,

Shuai

标签 (1)
0 项奖励
回复
0 回复数