Does SPIGen have a interface with LABView on MC33816?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does SPIGen have a interface with LABView on MC33816?

2,155件の閲覧回数
shuaiyue
Contributor I


Hey guys. I new to KIT 33816 board and I am using it to do the injection and control the pumping control valve. Now, I want to control the behavior of injection and pumping control valve in LABView since some feedback signals which are used to do a closed loop control come into the LABView. But here is problem, how can I run different single command or batch command automatically after I change the parameters in the configuration registers?

 

Best regards,

Shuai

ラベル(1)
0 件の賞賛
返信
0 返答(返信)