About MC33816 Vboost

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About MC33816 Vboost

5,734 Views
1334769096
Contributor II

I used the MC33816 IDE build the code for MC33816, but however I changed the Vboost voltage, from 24V to 65V. The Vboost always up to almost 80V, then the chip be broken. The mean is I can't control it. Can you help me? 

Thanks!

Labels (1)
7 Replies

5,617 Views
zflailfh
Contributor I

I also encountered the same problem, I can't control the Vboost,so I had to use a voltage regulator to protect the MC33816 from damage。

Does anyone know of a solution to this problem?

0 Kudos
Reply

5,617 Views
1334769096
Contributor II

Yep! I resolved it

5,617 Views
zflailfh
Contributor I

How did you solve it? (=^ ^=)

0 Kudos
Reply

5,617 Views
1334769096
Contributor II

Other configurations is default, The MC33816 IDE version is 2.3.1.0

0 Kudos
Reply

5,617 Views
guoweisun
NXP TechSupport
NXP TechSupport

Which kind of board do you test on? EVB or your own design board?

0 Kudos
Reply

5,617 Views
1334769096
Contributor II

my own design board, The schematic refers to the official demo.  And I wanna know If I used the default configurations on MC33816 IDE, Can I direct to test the board?

0 Kudos
Reply

5,617 Views
guoweisun
NXP TechSupport
NXP TechSupport

Suggest you test in EVB firstly,even if the default setting the Vboost can't up to 80V because of the maximum value is about 72V.

0 Kudos
Reply