About MC33816 Vboost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About MC33816 Vboost

5,712件の閲覧回数
1334769096
Contributor II

I used the MC33816 IDE build the code for MC33816, but however I changed the Vboost voltage, from 24V to 65V. The Vboost always up to almost 80V, then the chip be broken. The mean is I can't control it. Can you help me? 

Thanks!

ラベル(1)
7 返答(返信)

5,595件の閲覧回数
zflailfh
Contributor I

I also encountered the same problem, I can't control the Vboost,so I had to use a voltage regulator to protect the MC33816 from damage。

Does anyone know of a solution to this problem?

0 件の賞賛
返信

5,595件の閲覧回数
1334769096
Contributor II

Yep! I resolved it

5,595件の閲覧回数
zflailfh
Contributor I

How did you solve it? (=^ ^=)

0 件の賞賛
返信

5,595件の閲覧回数
1334769096
Contributor II

Other configurations is default, The MC33816 IDE version is 2.3.1.0

0 件の賞賛
返信

5,595件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Which kind of board do you test on? EVB or your own design board?

0 件の賞賛
返信

5,595件の閲覧回数
1334769096
Contributor II

my own design board, The schematic refers to the official demo.  And I wanna know If I used the default configurations on MC33816 IDE, Can I direct to test the board?

0 件の賞賛
返信

5,595件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Suggest you test in EVB firstly,even if the default setting the Vboost can't up to 80V because of the maximum value is about 72V.

0 件の賞賛
返信