which MPC processors support floating point operations

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

which MPC processors support floating point operations

786 次查看
herasmoiniguez
Contributor I

I like to know which processors support floating point operations

0 项奖励
回复
1 回复

676 次查看
Pavel
NXP Employee
NXP Employee

See the Section 3.1 in the MPC860 User's Manual:

https://www.nxp.com/docs/en/reference-manual/MPC860UM.pdf

 

See the Section 1.1.4.3 in the G2 LE core Reference Manual for the MPC82xx processors:

https://www.nxp.com/docs/en/reference-manual/G2CORERM.pdf

 

See the Section 1.1.3.2 in the E300 core Reference Manual for the MPC83xxx processors.

 

See also the following page about floating point on the e500 core for the MPC85xx processors:

https://en.wikipedia.org/wiki/PowerPC_e500


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复