tcp ip stack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tcp ip stack

1,382 Views
garimella
Contributor I

Like to port tcp ip stack into powerquicc mpc8309 processor without OS. Is it possible? If yes please suggest

0 Kudos
Reply
1 Reply

1,256 Views
alexander_yakov
NXP Employee
NXP Employee

I do not think this is "not possible" to port standalone tcp/ip stack to MPC8309 processor, however this is usually used for microcontrollers. As long as mpc8309 is not a "microcontroller", but processor from networking product segment, it is recommended to use it with Linux or other OS.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply