MPC 8250 SCC, Transparent Synchronous Operation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC 8250 SCC, Transparent Synchronous Operation?

1,372 Views
caryo_brien
Contributor III

We have a low-speed wan bridging requirement that needs the scc on a mpc8250 to run in transparent synchronous mode. Ideally we would be able to use a Linux driver for this.  There are drivers for hdlc mode, but not for unframed/transparent mode.  Any idea where I could find such a thing?  Or what I should use for a starting point?

0 Kudos
Reply
1 Reply

1,277 Views
Pavel
NXP Employee
NXP Employee

The MPC8250 SCC in transparent mode provides data transfers. Each clock can be supplied from the internal baud rate generator bank, DPLL output, or external pins. The SCC transparent data transfers is synchronous data transfers.

What Synchronous Operations are needed for your task?

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply