syntax error at line one

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

syntax error at line one

1,897 Views
maheshwarreddy
Fresh Out Contributor

we are using the code warrior  v8.8 in that while entering into debug that time we are getting an error .tha errors ccs log will be attached below .

Thank you

Best regards

Maheshwar reddy.

Tags (2)
0 Kudos
Reply
1 Reply

1,795 Views
Pavel
NXP Employee
NXP Employee

Test your connection of your TAP to the board.

Use /Tools/Hardware Diagnostics menu of CodeWarrior 8.8.

The MPC866 uses BDM connection (10pins) for debugging.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply