pl provide me command sequence to test I2C interface.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pl provide me command sequence to test I2C interface.

1,439 次查看
ranjeetsinha
Contributor I

i have to configure MPC8548 as I2C master. I want to test it at 100Kbps.

pl provide me command sequence.

0 项奖励
回复
2 回复数

1,312 次查看
andymastronardi
NXP Employee
NXP Employee

Ranjeet,

please see attached.

Andy

0 项奖励
回复

1,310 次查看
Pavel
NXP Employee
NXP Employee

See attached file. It is simple program I2C example for the MPC8548. It is CodeWarrior 9.8 project for the MPC8548CDS board.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复