pl provide me command sequence to test I2C interface.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pl provide me command sequence to test I2C interface.

1,914件の閲覧回数
ranjeetsinha
Contributor I

i have to configure MPC8548 as I2C master. I want to test it at 100Kbps.

pl provide me command sequence.

0 件の賞賛
返信
2 返答(返信)

1,787件の閲覧回数
andymastronardi
NXP Employee
NXP Employee

Ranjeet,

please see attached.

Andy

0 件の賞賛
返信

1,785件の閲覧回数
Pavel
NXP Employee
NXP Employee

See attached file. It is simple program I2C example for the MPC8548. It is CodeWarrior 9.8 project for the MPC8548CDS board.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信