ping test on Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ping test on Ethernet

3,129 Views
vadrevujyothi
Contributor I

Hi,

 

             I am jyothi. I have installed U-boot 1.1.6 in MPC8323 development board. Ethernet is not pinging to my windows system. Can you help me out for anything i missed configuration of environment variables. I am attaching the environment variables which i have configured.

Original Attachment has been moved to: u-boot.txt.zip

Labels (1)
0 Kudos
Reply
5 Replies

2,271 Views
alexander_yakov
NXP Employee
NXP Employee

Ok, thank you for clarification. MPC8323EVRAFDC is processor partnumber, but not board name. Please specify board name.

Also, how exactly you are doing this test? Could you please describe your test procedure as precise as possible, so just to reproduce it here in lab?

0 Kudos
Reply

2,271 Views
vadrevujyothi
Contributor I

K.Board name is MPC8323E-RDB. I have connected ethernet port of this board

to my windows 7 PC directly. I tried to ping from PC to board ip address

but Its not pinging to my PC. And also i tried to ping from my board with

same ip address then also it is not working . Once again I am attaching

Configuration of environment variables. Can you tell me any other problem

is there?

On Tue, Sep 20, 2016 at 12:27 PM, alexander.yakovlev <

0 Kudos
Reply

2,271 Views
alexander_yakov
NXP Employee
NXP Employee

1. Connecting "directly" may not work - for direct board to PC connection without using ethernet switch you need specific "crossover" ethernet patch cord. If you do not have this patch cord than please try connecting through ethernet switch.

2. Ping from PC to U-boot in not supported by U-boot, the only ping from U-boot to PC is supported.

3. Please make sure you have disabled windows firewall or enabled ping rule in firewall.

4. Please do not forget to check "link" led for connection status before pinging.

I do not see anything incorrect in your attached file. In case if you are using our board and our BSP, than you do not need to make any changes in U-boot settings, standard prebuilt image should work.

0 Kudos
Reply

2,271 Views
alexander_yakov
NXP Employee
NXP Employee

Could you please answer the following questions:

1. Which board you are using?

2. Which Linux BSP you are using?

0 Kudos
Reply

2,271 Views
vadrevujyothi
Contributor I

I am using MPC8323EVRAFDC development board. And I am using freescale

MPC8323E BSP Version: 1.0-rt (7-2-1-rt) featuring Linux 2.6.20.6-rt8.

On Mon, Sep 19, 2016 at 8:53 PM, alexander.yakovlev <

0 Kudos
Reply