mpc8379 vsc7385

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mpc8379 vsc7385

1,611 次查看
jfsong1
Contributor I

hello, where can I find the source code of VSC7385 in the mpc8379 BSP which contains vsc2bin ?  I am wrong in using the switch led pin functions which indicate 1000Mbps and Tx. I want to reassign the led pin definitions through changing the source code of VSC7385 . If possible, any other simple methods will be preferred except changing source code. Thank you .

0 项奖励
回复
2 回复数

1,483 次查看
ufedor
NXP Employee
NXP Employee

VSC7385 is not an NXP product. We neither develop, nor distribute source codes for it. The firmware binary included in the BSP is a standard unmanaged switch firmware that was available from Vitesse at the moment of the BSP development.

0 项奖励
回复

1,483 次查看
jfsong1
Contributor I

Thanks  a lot.

0 项奖励
回复