hello, where can I find the source code of VSC7385 in the mpc8379 BSP which contains vsc2bin ? I am wrong in using the switch led pin functions which indicate 1000Mbps and Tx. I want to reassign the led pin definitions through changing the source code of VSC7385 . If possible, any other simple methods will be preferred except changing source code. Thank you .
VSC7385 is not an NXP product. We neither develop, nor distribute source codes for it. The firmware binary included in the BSP is a standard unmanaged switch firmware that was available from Vitesse at the moment of the BSP development.
Thanks a lot.