mpc8379 vsc7385

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpc8379 vsc7385

1,603件の閲覧回数
jfsong1
Contributor I

hello, where can I find the source code of VSC7385 in the mpc8379 BSP which contains vsc2bin ?  I am wrong in using the switch led pin functions which indicate 1000Mbps and Tx. I want to reassign the led pin definitions through changing the source code of VSC7385 . If possible, any other simple methods will be preferred except changing source code. Thank you .

0 件の賞賛
返信
2 返答(返信)

1,475件の閲覧回数
ufedor
NXP Employee
NXP Employee

VSC7385 is not an NXP product. We neither develop, nor distribute source codes for it. The firmware binary included in the BSP is a standard unmanaged switch firmware that was available from Vitesse at the moment of the BSP development.

0 件の賞賛
返信

1,475件の閲覧回数
jfsong1
Contributor I

Thanks  a lot.

0 件の賞賛
返信