mpc8360 risc timer clocking

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpc8360 risc timer clocking

3,763件の閲覧回数
eric2013
Fresh Out Contributor

In QEIWRM - 5.10.5 Timer Functional Description:

The clock input to the timer prescaler can be selected from the following sources:

• The system clock (ipg_clock)

• The system ‘slow go’ clock (ipg_clock internally divided by 16)

What does the "system clock" mean? Is it csb_clk, or ce_clk, or core_clk, or the PCI_CLK ( CLKIN not used)?

Thanks.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,473件の閲覧回数
LPP
NXP Employee
NXP Employee

ipg_clock is global IP clock. In case of MPC8360, ipg_clock = csb_clk

0 件の賞賛
返信

3,473件の閲覧回数
eric2013
Fresh Out Contributor

Thanks. But I got one different answer from Technical Support that  the "ipg_clock = one half of the QUICC Engine frequency" and the "QUICC Engine frequency" is the ce_clk.

0 件の賞賛
返信

3,473件の閲覧回数
LPP
NXP Employee
NXP Employee

You are right. The link is QEIWRM Rev. 4.4, section 5.10.2.2 GTM Clock Source Modes.

Please accept my apology for this inconsistence.

0 件の賞賛
返信

3,468件の閲覧回数
eric2013
Fresh Out Contributor

Thanks,LPP.

0 件の賞賛
返信