mpc8360 risc timer clocking

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc8360 risc timer clocking

3,681 Views
eric2013
Contributor I

In QEIWRM - 5.10.5 Timer Functional Description:

The clock input to the timer prescaler can be selected from the following sources:

• The system clock (ipg_clock)

• The system ‘slow go’ clock (ipg_clock internally divided by 16)

What does the "system clock" mean? Is it csb_clk, or ce_clk, or core_clk, or the PCI_CLK ( CLKIN not used)?

Thanks.

Labels (1)
0 Kudos
Reply
4 Replies

3,391 Views
LPP
NXP Employee
NXP Employee

ipg_clock is global IP clock. In case of MPC8360, ipg_clock = csb_clk

0 Kudos
Reply

3,391 Views
eric2013
Contributor I

Thanks. But I got one different answer from Technical Support that  the "ipg_clock = one half of the QUICC Engine frequency" and the "QUICC Engine frequency" is the ce_clk.

0 Kudos
Reply

3,391 Views
LPP
NXP Employee
NXP Employee

You are right. The link is QEIWRM Rev. 4.4, section 5.10.2.2 GTM Clock Source Modes.

Please accept my apology for this inconsistence.

0 Kudos
Reply

3,386 Views
eric2013
Contributor I

Thanks,LPP.

0 Kudos
Reply