hello,
I use two mpc8309 ,one as master pci device,another as agent pci device, all run linux OS, my board is likely mpc8309-SOM board. i configure master pci device's outbound like this under uboot(uboot version is u-boot-2010.06 ):
/*
#define CONFIG_SYS_PCI1_MEM_BASE 0x80000000
#define CONFIG_SYS_PCI1_MEM_PHYS CONFIG_SYS_PCI1_MEM_BASE
#define CONFIG_SYS_PCI1_MEM_SIZE 0x10000000 /* 256M */
static struct pci_region pci_regions[] = {
{
bus_start: CONFIG_SYS_PCI1_MEM_BASE,
phys_start: CONFIG_SYS_PCI1_MEM_PHYS,
size: CONFIG_SYS_PCI1_MEM_SIZE,
flags: PCI_REGION_MEM | PCI_REGION_PREFETCH
},
{
bus_start: CONFIG_SYS_PCI1_MMIO_BASE,
phys_start: CONFIG_SYS_PCI1_MMIO_PHYS,
size: CONFIG_SYS_PCI1_MMIO_SIZE,
flags: PCI_REGION_MEM
},
{
bus_start: CONFIG_SYS_PCI1_IO_BASE,
phys_start: CONFIG_SYS_PCI1_IO_PHYS,
size: CONFIG_SYS_PCI1_IO_SIZE,
flags: PCI_REGION_IO
}
};
#ifdef CONFIG_PCI
void pci_init_board(void)
{
volatile immap_t *immr = (volatile immap_t *)CONFIG_SYS_IMMR;
volatile clk83xx_t *clk = (volatile clk83xx_t *)&immr->clk;
volatile law83xx_t *pci_law = immr->sysconf.pcilaw;
struct pci_region *reg[] = { pci_regions };
/* Enable all 3 PCI_CLK_OUTPUTs. */
clk->occr |= 0xe0000000;
/* Configure PCI Local Access Windows */
pci_law[0].bar = CONFIG_SYS_PCI1_MEM_PHYS & LAWBAR_BAR;
pci_law[0].ar = LBLAWAR_EN | LBLAWAR_512MB;
pci_law[1].bar = CONFIG_SYS_PCI1_IO_PHYS & LAWBAR_BAR;
pci_law[1].ar = LBLAWAR_EN | LBLAWAR_1MB;
mpc83xx_pci_init(1, reg, 0);
puts("PCI: Master mode enabled\n");
}
#endif
static void pci_init_bus(int bus, struct pci_region *reg)
{
volatile immap_t *immr = (volatile immap_t *)CONFIG_SYS_IMMR;
volatile pot83xx_t *pot = immr->ios.pot;
volatile pcictrl83xx_t *pci_ctrl = &immr->pci_ctrl[bus];
struct pci_controller *hose = &pci_hose[bus];
u32 dev;
u16 reg16;
int i;
if (bus == 1)
pot += 3;
/* Setup outbound translation windows */
for (i = 0; i < 3; i++, reg++, pot++) {
if (reg->size == 0)
break;
hose->regions[i] = *reg;
hose->region_count++;
pot->potar = reg->bus_start >> 12;
pot->pobar = reg->phys_start >> 12;
pot->pocmr = ~(reg->size - 1) >> 12;
if (reg->flags & PCI_REGION_IO)
pot->pocmr |= POCMR_IO;
#ifdef CONFIG_83XX_PCI_STREAMING
else if (reg->flags & PCI_REGION_PREFETCH)
pot->pocmr |= POCMR_SE;
#endif
if (bus == 1)
pot->pocmr |= POCMR_DST;
pot->pocmr |= POCMR_EN;
}
hose->first_busno = pci_last_busno() + 1;
hose->last_busno = 0xff;
pci_setup_indirect(hose, CONFIG_SYS_IMMR + 0x8300 + bus * 0x80,
CONFIG_SYS_IMMR + 0x8304 + bus * 0x80);
pci_register_hose(hose);
/*
* Write to Command register
*/
reg16 = 0xff;
dev = PCI_BDF(hose->first_busno, 0, 0);
pci_hose_read_config_word(hose, dev, PCI_COMMAND, ®16);
reg16 |= PCI_COMMAND_SERR | PCI_COMMAND_MASTER | PCI_COMMAND_MEMORY;
pci_hose_write_config_word(hose, dev, PCI_COMMAND, reg16);
/*
* Clear non-reserved bits in status register.
*/
pci_hose_write_config_word(hose, dev, PCI_STATUS, 0xffff);
pci_hose_write_config_byte(hose, dev, PCI_LATENCY_TIMER, 0x80);
pci_hose_write_config_byte(hose, dev, PCI_CACHE_LINE_SIZE, 0x08);
#ifdef CONFIG_PCI_SCAN_SHOW
printf("PCI: Bus Dev VenId DevId Class Int\n");
#endif
#ifndef CONFIG_PCISLAVE
/*
* Hose scan.
*/
hose->last_busno = pci_hose_scan(hose);
#endif
}
configure agent pci device's inbound like this under uboot(uboot version is u-boot-2010.06 ):
#define CONFIG_SYS_PCI1_MEM_BASE 0x80000000
#define CONFIG_SYS_PCI1_MEM_PHYS CONFIG_SYS_PCI1_MEM_BASE
#define CONFIG_SYS_PCI1_MEM_SIZE 0x10000000 /* 256M */
static struct pci_region pci_regions[] = {
{
bus_start: CONFIG_SYS_PCI1_MEM_BASE,
phys_start: CONFIG_SYS_PCI1_MEM_PHYS,
size: CONFIG_SYS_PCI1_MEM_SIZE,
flags: PCI_REGION_MEM | PCI_REGION_PREFETCH
},
{
bus_start: CONFIG_SYS_PCI1_MMIO_BASE,
phys_start: CONFIG_SYS_PCI1_MMIO_PHYS,
size: CONFIG_SYS_PCI1_MMIO_SIZE,
flags: PCI_REGION_MEM
},
{
bus_start: CONFIG_SYS_PCI1_IO_BASE,
phys_start: CONFIG_SYS_PCI1_IO_PHYS,
size: CONFIG_SYS_PCI1_IO_SIZE,
flags: PCI_REGION_IO
}
};
#ifdef CONFIG_PCISLAVE
/void pci_init_board(void)
{
volatile immap_t *immr = (volatile immap_t *)CONFIG_SYS_IMMR;
volatile law83xx_t *pci_law = immr->sysconf.pcilaw;
volatile pcictrl83xx_t *pci_ctrl = &immr->pci_ctrl[0];
struct pci_region *reg[] = { pci_regions };
/* Configure PCI Local Access Windows */
pci_law[0].bar = CONFIG_SYS_PCI1_MEM_PHYS & LAWBAR_BAR;
pci_law[0].ar = LAWAR_EN | LBLAWAR_512MB;
mpc83xx_pci_init(1, reg, 0);
/* Configure PCI Inbound Translation Windows (3 1MB windows) */
pci_ctrl->pitar0 = 0x0;
pci_ctrl->pibar0 = 0x0;
pci_ctrl->piwar0 = PIWAR_EN | PIWAR_PF | PIWAR_RTT_SNOOP | PIWAR_WTT_SNOOP | PIWAR_IWS_1M;
/* Unlock the configuration bit */
mpc83xx_pcislave_unlock(0);
/printf("PCI: Agent mode enabled\n");
}
static void pci_init_bus(int bus, struct pci_region *reg)
{
volatile immap_t *immr = (volatile immap_t *)CONFIG_SYS_IMMR;
volatile pot83xx_t *pot = immr->ios.pot;
volatile pcictrl83xx_t *pci_ctrl = &immr->pci_ctrl[bus];
struct pci_controller *hose = &pci_hose[bus];
u32 dev;
u16 reg16;
int i;
if (bus == 1)
pot += 3;
/* Point inbound translation at RAM */
pci_ctrl->pitar1 = 0;
pci_ctrl->pibar1 = 0;
pci_ctrl->piebar1 = 0;
pci_ctrl->piwar1 = PIWAR_EN | PIWAR_PF | PIWAR_RTT_SNOOP |
PIWAR_WTT_SNOOP | (__ilog2(gd->ram_size - 1));
i = hose->region_count++;
hose->regions[i].bus_start = 0;
hose->regions[i].phys_start = 0;
hose->regions[i].size = gd->ram_size;
hose->regions[i].flags = PCI_REGION_MEM | PCI_REGION_SYS_MEMORY;
hose->first_busno = pci_last_busno() + 1;
hose->last_busno = 0xff;
pci_setup_indirect(hose, CONFIG_SYS_IMMR + 0x8300 + bus * 0x80,
CONFIG_SYS_IMMR + 0x8304 + bus * 0x80);
pci_register_hose(hose);
/*
* Write to Command register
*/
reg16 = 0xff;
dev = PCI_BDF(hose->first_busno, 0, 0);
pci_hose_read_config_word(hose, dev, PCI_COMMAND, ®16);
reg16 |= PCI_COMMAND_SERR | PCI_COMMAND_MASTER | PCI_COMMAND_MEMORY;
pci_hose_write_config_word(hose, dev, PCI_COMMAND, reg16);
/*
* Clear non-reserved bits in status register.
*/
pci_hose_write_config_word(hose, dev, PCI_STATUS, 0xffff);
pci_hose_write_config_byte(hose, dev, PCI_LATENCY_TIMER, 0x80);
pci_hose_write_config_byte(hose, dev, PCI_CACHE_LINE_SIZE, 0x08);
#ifdef CONFIG_PCI_SCAN_SHOW
printf("PCI: Bus Dev VenId DevId Class Int\n");
#endif
#ifndef CONFIG_PCISLAVE
/*
* Hose scan.
*/
hose->last_busno = pci_hose_scan(hose);
#endif
}
master device can write and read 0x80000000 ~0x80100000, agent can read and write 0x0~0x100000.
i think mapping like this

but i don't want to use pitar is 0x0 ,i want use pitar is 0x80000000, i configure pci_ctrl->pitar1 = 0x80000000, pci don't working ,please give me some advices.
Thanks.