We recommend using toolchain from NXP SDK Yocto Linux for application building.
- 1. Install toolchain use command sequence below and see the following page:
(https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-16DBC8E2-9A18-4867-9BE1-1...).
Build and install the standalone toolchain with Yocto:
$ source ./fsl-setup-poky -m <machine>
$ bitbake fsl-toolchain
$ cd build_<machine>_release/tmp/deploy/sdk
$ ./fsl-networking-eglibc-<host-system>-<core>-toolchain-<release>.sh
Note: The default installation path for standalone toolchain is /opt/fsl-networking/. The install folder can be specified during the installation procedure.
Use the following command sequence if SDK 1.9 is used:
source /opt/fsl-qoriq/1.9/environment-setup-ppce500v2-fsl-linux-gnuspe
Check result of "source" command. Use "$PATH" command. The "source" command should add path to gcc compiler.
You should see similar message:
$PATH
bash: /opt/fsl-qoriq/1.9/sysroots/x86_64-fslsdk-linux/usr/bin:/opt/fsl-qoriq/1.9/sysroots/x86_64-fslsdk-linux/usr/bin/powerpc-fsl-linux-gnuspe:
$CC test.c --sysroot=/opt/fsl-qoriq/1.9/sysroots/ppce500v2-fsl-linux-gnuspe -o test.elf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------