hi,
right now we are looking for a processor which is should have following features single/ duel core of specifications 3.3DMIPS/Mhz and DDR3 support and has to operate industrial temperature (-40 to +105 degree) 32/64 bit operation and 1Ghz and more frequency
thanks
phanikumar
Have a great day,
It is PowerQUICC Processors community page. So I suppose you asked for a PowerPC processor. I think the T10xx are close to your requirements. See list on
For example T1013NXN7PQA (https://www.nxp.com/part/T1013NXN7PQA) characteristics are 1xCPU 64-Bit Pwr Arch (E5500 core), 1.4GHz, DDR3L/4 controller, PCIe, 1/10GbE, -40 to 105 C
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------