is there any processor available with single core of specifications 3.3DMIPS/Mhz and ddr3 support and has to operate industrial temperature (-40 to +105 degree)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is there any processor available with single core of specifications 3.3DMIPS/Mhz and ddr3 support and has to operate industrial temperature (-40 to +105 degree)

809 Views
phanikumarkorla
Contributor I

hi,

right now we are looking for a processor which is should have following features single/ duel core of specifications 3.3DMIPS/Mhz and DDR3 support and has to operate industrial temperature (-40 to +105 degree) 32/64 bit operation and  1Ghz and more frequency

thanks

phanikumar

0 Kudos
Reply
1 Reply

727 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

It is PowerQUICC Processors community page. So I suppose you asked for a PowerPC processor. I think the T10xx are close to your requirements. See list on

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/qoriq-pla...

For example T1013NXN7PQA (https://www.nxp.com/part/T1013NXN7PQA) characteristics are 1xCPU 64-Bit Pwr Arch (E5500 core), 1.4GHz, DDR3L/4 controller, PCIe, 1/10GbE,  -40 to 105 C

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply