interrupts examples for MPC8309

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

interrupts examples for MPC8309

661 次查看
garimella
Contributor I

Any good examples (both standalone and kernel mode) to demonstrate interrupt processing for MPC8309.

0 项奖励
回复
1 回复

559 次查看
Pavel
NXP Employee
NXP Employee

See attached file. It is standalone interrupt program example for the MPC8349. Use similar code on the MPC8309 board. It is CodeWarrior example.

Usually Linux driver precedes interrupts. See driver code for interrupt in kernel mode.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复