interrupts examples for MPC8309

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

interrupts examples for MPC8309

950件の閲覧回数
garimella
Contributor I

Any good examples (both standalone and kernel mode) to demonstrate interrupt processing for MPC8309.

0 件の賞賛
返信
1 返信

848件の閲覧回数
Pavel
NXP Employee
NXP Employee

See attached file. It is standalone interrupt program example for the MPC8349. Use similar code on the MPC8309 board. It is CodeWarrior example.

Usually Linux driver precedes interrupts. See driver code for interrupt in kernel mode.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信