hi
my demo board is P2020DS , i use the sdk1.6. I want use the p2020ds as NTP server , how to include the NTP server module and configuration? thank U.
root@p2020ds:~# date -R Mon, 10 Aug 2020 10:13:11 +0000 root@p2020ds:~# root@p2020ds:~# root@p2020ds:~# root@p2020ds:~# ntpd BusyBox v1.22.1 (2020-08-10 01:44:42 PDT) multi-call binary. Usage: ntpd [-dnqNwl] [-S PROG] [-p PEER]... root@p2020ds:~#
Please add "ntp" in IMAGE_INSTALL variable in meta-fsl-networking/images/fsl-image-core.bb.
IMAGE_INSTALL += " \ packagegroup-fsl-core \ ntp \"
Then rebuild rootfs filesystem with the following command.
$ bitbake fsl-image-core
hi Yiping Wang
I have done as ur suggestion. but thers is no /etc/ntp.conf and how can I config p2020ds as NTP service ? c an u give me some suggestion?
root@p2020ds:/# service ntpd start -sh: service: command not found root@p2020ds:/#
/etc# ntp.conf -sh: ntp.conf: command not found root@p2020ds:/etc# root@p2020ds:/etc# root@p2020ds:/etc# root@p2020ds:/etc# root@p2020ds:/etc# root@p2020ds:/etc# cd .. root@p2020ds:/# ntpd -p 192.168.5.12 -qNn ntpd: time slew +0.000000s
add
ntpd -p 192.168.1.16 -qNn
root@p2020ds:/# /etc/init.d/ntpd star
Starting ntpd: /usr/sbin/ntpd is already running 2415 done root@p2020ds:/# netstat -ln|grep 123 udp 0 0 192.168.1.16:123 0.0.0.0:* udp 0 0 127.0.0.1:123 0.0.0.0:* udp 0 0 0.0.0.0:123 0.0.0.0:* udp6 0 0 fe80::2e0:cff:fe02::123 :::* udp6 0 0 ::1:123 :::* udp6 0 0 :::123 :::* root@p2020ds:/# ntpstat -sh: ntpstat: command not found root@p2020ds:/#
Please execute the following commands.
/etc/init.d/ntpd restart
add problem, why service: command not found ? thank u.
2409 ttyS0 00:00:00 sh 2415 ? 00:00:00 ntpd 2424 ttyS0 00:00:00 ps root@p2020ds:/# service stop ntpd -sh: service: command not found root@p2020ds:/#