ftp and tftp in uboot and vxworks kernel in t2080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ftp and tftp in uboot and vxworks kernel in t2080

1,052 Views
monalihaware
Contributor III

i have loaded uboot in t2080. And using ethernet marvel PHY 88E1512 in it.

Vx works is loaded on top of it using tftp. But ftp is not working after loadinf vxworks.

What could be the problem. If ethernet had any problem, even tftp would not have worked as per my understanding. Then what could be the reason for ftp not working. Can any one help?

0 Kudos
Reply
1 Reply

1,018 Views
yipingwang
NXP TechSupport
NXP TechSupport

If tftp can work in u-boot, it means there is no problem with Ethernet port.

Do you mean ftp doesn't work in Vxworks environment?

If so, you need to contact WindRiver.

0 Kudos
Reply