codewarrior v8.8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior v8.8

2,397 Views
venkat1
Contributor III

Hi all,

I am working on MPC8358 Power architecture processor using Codewarrior v8.8 IDE. while configuring init file in Codewarrior setup window but  its not updating in .asm or in any related file.

 

please tell me what would be the problem for this?

 

Regards,

Venkat

0 Kudos
Reply
2 Replies

2,389 Views
yipingwang
NXP TechSupport
NXP TechSupport

For MPC8358 custom board bring up, you need to modify initialization file  PowerPC_EABI_Support\Initialization_Files\PQ2\8360MDS_rev1_init.cfg based on your target board.

Please create a bareboard project for MPC8358 in CodeWarrior IDE, in "Select processor and board" panel, please select processor PowerPC 8358 and board 8360MDS(rev1).

Then modify initialization file in CodeWarrior IDE from Edit->Debug Version Settings->Debugger->EPPC Debugger Settings->Use Target Initialization File.

0 Kudos
Reply

2,372 Views
venkat1
Contributor III

sir, I have followed the above process but the .cfg file is not updating into the project code.

please tell me, what will be the problem?

0 Kudos
Reply