about mpc8358 proccessor interface with DDR SDRAM.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

about mpc8358 proccessor interface with DDR SDRAM.

1,083 次查看
venkat1
Contributor III

Hello All,

    We are using MPC8358, PowerQUICC II Pro family of Processor in our design.

    Require Tech material or ref SCH in interfacing the MPC8358 Processor with DDR SDRAM.

REgards,

Venkat

8495952871

Balaji

98862 01027

3 回复数

973 次查看
Bulat
NXP Employee
NXP Employee

The only available schematic example is the schematics of the 'MPC8360EA Modular Development System', MPC8360EAMDS:

https://www.nxp.com/downloads/en/schematics/MPC8360EAMDSSCH.pdf 

This board uses two SODIMMs interfaced to the MPC8360 to get functionality of two memory controllers. In your case (MPC8358, single memory controller) you need to take a look at U33 SODIMM only.

Note also that TBGA package is used in the schematics, if you are going to use PBGA package, pin numbering needs to be changed.

Regards,

Bulat

973 次查看
venkat1
Contributor III

Thank you. mr.Bulat Karymov.

we are using two  ddr sdram  size of  256Mb (16M16 config.) for achieving 32-bit data bus.  please suggest us how this  cs#  and logical banks  config.? so that we communicate 32-bit data with sdram and mpc8358 ..

thank you regards,

venkat.

0 项奖励
回复

973 次查看
Bulat
NXP Employee
NXP Employee

You need to use a single CS (CS0) and four byte lanes (MDQ0..MDQ31) for your configuration.

Regards,

Bulat